.
| YOU WILL NEED: LED green Resistor 330R Switch SPST panel mount 6" of wire 9V battery and battery clip 1-3/4" PVC pipe, 6-1/2" long |
3/16" balsa wood sheet, 6" x 4" 3/8" x 1/2" balsa wood stick, 4" long Heat-shrink tubing (optional) Saw Wire cutters Wire strippers |
Sharp knife Hot glue gun Solder Soldering iron Download templates from: makezine.com/16/123_alien |
|
1. Build The Basic Circuit. Trim the resistor and LED leads to 1/4" long, and solder 1 end of the resistor onto the negative lead of the LED. Cut about 6" of wire, and solder it to the positive lead of the LED. Put a piece of heat-shrink tubing over the black (negative) wire of the 9V battery clip, then solder the wire to the other leg of the resistor. Solder the red (positive) wire from the battery clip to the middle terminal of the switch. Place heat-shrink tubing over this wire if you wish. Solder the positive LED wire to one of the outside pins of the switch. 2. Build The Case Parts. Print the templates of the front and back plates, cut them out, and tape them to the balsa wood sheet. With a sharp knife, cut out the inside of the template first, then the outside. Use the cross on the back template to mark the hole for the switch. Cut two 1-3/4" lengths of balsa wood stick. With the knife, drill a 3/16" hole in the middle of one, and a 1/4" hole in the middle of the other. Drill a 1/4" hole in the middle of the balsa back plate where it's marked, then glue the stick with the 1/4" hole to the back plate. 3. Put It All Together. Glue the LED into the stick with the 6" hole. Fit the switch to the back plate. Fit the LED stick into the middle of the PVC pipe, then glue the front plate onto the pipe. Snap the battery into the battery clip, then fit the back plate into place. To set up the projector, place it in a dark room 1'- 4' from the wall. Move it closer to the wall for a smaller image, and farther away for a bigger image. The best thing about this project is that you can cut out any simple image and project it onto the wall, perhaps pumpkins for Halloween and a tree for Christmas. |
![]() ![]()
|
Written by Brian McNamara Make Magazine Volume 16, page 104