Altoids USB Charger |
![]() |
Has your phone or iPod ever died when you needed it the most? That's why I designed a quick little battery charger for your electronics! Just plug your device into its USB port, turn it on, and you're all set! Best yet, it all fits in an Altoids gum tin!
|
The Design Lots of electronics are powered from a USB cable, so I figured that a powered USB port would be the most useful power source. I used a voltmeter to measure the voltage on each of the pins on my iPod AC Adapter, and wound up with +5.16V on the V+ pin, +2.06V on the D- pin, and +2.76V on the D+ pin. I'm using a 7805 voltage regulator to get +5V for V+, and am using two resistors for each data pin. I calculated the resistor values to minimize current loss (as not much current needs to go to each data pin). Here's the schematic: Parts You Will Need Assembly For simplicity, I decided to just twist the leads together, as the circuit is pretty simple. You may want to solder them into a prototyping board for durability; see instructions for that below. To twist the leads together, you'll need to solder wires to the switch, the regulator, and the USB socket. Then twist the red lead from the battery with one of the wires on the switch, and twist the other lead from the switch onto the left wire (with the regulator's metal part down) on the voltage regulator. Then, twist the rightmost wire on the regulator with the two 27kΩ resistor and the lead from pin 1 of the USB socket. After that, twist the lead from pin 2 of the USB socket with the other end of one of the 27kΩ resistors and the 22kΩ resistor. Then twist the other end of the second 27kΩ resistor with the lead from pin 3 of the USB socket and one end of the 39kΩ resistor. Finally, twist the lead from pin 4 of the USB socket with the remaining ends of the battery, the regulator, and the 22kΩ and 39kΩ resistors. You should have a functional mess of twisted wires at this point, so test the circuit by plugging in a device or by using a volt meter. If it doesn't work, check the switch and your wiring. Once it works, wrap each twist with a length of electrical tape. Then cut a USB sized hole in the Altoids tin with the metal shears. You only need to cut down twice, then just bend the metal repeatedly until it snaps. I'd suggest covering the edges with some electrical tape; it can be sharp! Then put the battery in the tin and push the USB socket through the hole. Then, push the rest of the circuit in the remaining space; it should fit pretty easily. It looked pretty messy, so I covered up the guts of the device with some electrical tape. And voila! You have a working charger! |
![]() ![]() ![]() Figure 3. USB Pin out Diagram, looking into the socket. ![]() |
![]() |
![]() |
Going Further
If you want, you can put the circuit on a prototyping board; It'll be smaller and It'll look simpler, but It will be a little more complicated to make. It shouldn't be too much of a problem; there are just four resistors and a switch to put in. The USB socket's leads are 0.1" apart and will fit right into a proto board.
iPod is a trademark of Apple Inc. Altoids and the Altoids logo are trademarks of Callard & Bowser Inc.
About the author
Phil Tang is an engineering student at Tufts University and a summer intern at Jameco, working on new media and data integrity. He loves learning a little bit about everything and a lot about the interesting bits. He's a proficient roboticist and all-around computer guy, enjoying all kinds of electronic marvels. He can be reached at phil.sj.tang@gmail.com.