Frog Feeder

By Rik Sagar

I wanted to design a way to automatically feed my son's pet frogs while we were out of town.

The frogs need to be fed every two days, and I couldn't find anything in the store to feed them automatically.

The project requires software on an Arduino and some simple circuit construction, including soldering. Some mechanical construction is required to mount the motor, sensors and electronics, but the whole project can be done with basic mechanical skills.

Overview

This project was designed to automatically feed my son's pet frogs while we were out of town for two weeks.

The frogs need to be fed once every two days and no commercial frog feeder was available. A fish feeder, purchased from PetCo, was considered as an "off the shelf solution," but it didn't work. The fish feeder was however cannibalized for parts for this project. The project required software on an Arduino and some simple circuitry, soldered onto a protoboard. Some mechanical construction was required to mount the motor, sensors and electronics, but the whole project can be done with basic mechanical skills.

How it Works

An Arduino is used to feed the frogs once every two days. The Arduino counts down the necessary number of seconds for two days (configurable in the software). Once this time has passed, an output pin on the Arduino drives a motor, which rotates a hopper to dump food into the frog tank.
Frog Feeder

A sensor, monitoring the food hopper, detects when the hopper has dumped the food and the Arduino turns off the motor. The cycle repeats indefinitely.

Circuit Design

Motor Drive Circuit

The motor and gearbox are an off-the-shelf, low voltage kit. The motor requires voltage around 3-5volts and has a low current requirement. The motor is driven through a medium power transistor (TR1). An opto-isolator (IC1) is used to interface between the Arduino and TR1. The opto-isolator provides noise isolation and reduces the risks of causing damage to the Arduino due to short-circuits. I/O line 12 on the Arduino is used to drive the motor control circuit.

Position Sensor

The small DC motor driving the hopper tends to start slowly when power is applied, so it takes some time to get to speed. It also over-shoots when power is removed, so the time for a complete revolution is not constant. Additionally, the food hopper tends to "slip" under load (a deliberate part of its design?) adding to the timing variability. For these reasons, the only way to know when food has been delivered is to monitor the food hopper and wait until it completes a full revolution. To monitor the food hopper a photo interrupter (IC2) detects a tab attached to the food hopper. The sensor is simply an IR emitter/receiver pair with an air gap between them. Anything passing through the air gap causes the sensor output to transition high-to-low. The output of IC2 connects between I/O pin 11 on the Arduino and the Arduino's ground. As with the motor drive circuit, this sensor is electrically isolated from the Arduino power supplies.

Assembly

The circuit was soldered onto the "Phenolic" prototyping board. Jumper leads from the circuit connect to the Arduino board via a 4 pin header providing connections to I/O pins 11, 12 and GND.

Software Design

A short program on the Arduino implements a state machine. The state machine waits for 2 days, starts the motor, monitors the sensor, stops the motor, then resets the timer to repeat the process 2 days later. The program will loop forever.

As with all Arduino programs there is a set-up function (setup ( ) ) and a function for the main-loop (loop ( ) ). The set-up function executes once, when the software first starts, the mainloop is called repeatedly while the Arduino is in the normal running state. In addition to those two functions, there are declarations of a number of global variables, macros and some enumerations (custom data types).

Declarations

Motor Drive Circuit

position sensor

assembly

The first block of code is the declaration of variables and values needed for the application. This is done at the top of the file so the values can be used thoughout the application. This avoids using hardcoded values in the code, for example for things like seconds in a day or the pin numbers of the outputs.
• Lines 10-12: Variables identifying the pins used for inputs and outputs
• Lines 17-30: Macros and defines used to control timing. FEED_INTERVAL - defines how long between feedings
  MAX_DELIVERY_DURATION – limit the maximum time the motor will remain on
• Lines 35-50: Application variables and state machine definition. next_feeding/feeding_timer – Control when the next
  feeding occurs and when it stops. FeedState/feed_state – enumerated type declaring the states of a state machine used
  in the main loop to control the application. motorDetect/lastMotorDetect – Read the photo interrupter and detect the end
  of a revolution.


Setup

The setup ( ) function sets the modes of the input and output pins, and initializes the outputs. The setup function initializes the application state machine and sets an intial feeding for 10 seconds into the future.

Main Loop

The loop ( ) function operates the state machine. The state machine has three states: Waiting for Feeding; Delivering Food; and Finishing Feeding.

In Waiting for Feeding the state machine checks the time against the next feeding time. Once the next feeding time is reached this state turns on the motor to deliver the food, then transitions to the Delivering Food state.

In Delivering Food the state machine checks for the photo interrupter to generate a low to high transition, signaling the tab has passed though the interrupter. Once the low-high tranisiton is detected, the state machine transitions to Finishing Feeding.

Additionally, in Delivering Food, the state machine checks whether the motor has been running for more than MAX_DELIVERY_DURATION seconds. If that is the case, the state machine transitions to Finishing Feeding.

In Finishing Feeding, the motor is stopped, the next feeding time is calculated (FEED_INTERVAL seconds after the last feeding time), and the state machine transitions back to Waiting for Feeding.

The state machine is implemented simply as a switch statement, with three cases.

Also in the loop ( ) function the LED on the Arduino board is made to flash briefly once per second, to show that the application is still running normally.

Enhancements

The performance of the food hopper is, to say the least, disappointing. So, one alteration I am considering is a hopper with a Screw Conveyor. The food hopper is unnecessarily complex and unreliable. A screw conveyor should be a more accurate, less error prone and cheaper solution ($5 rather than the $20 I paid for the fish feeder).

Mechanical Design

As the pictures show, the mechanical design of the project is very much a prototype. Once the design is adapted to use the screw conveyor a better housing can be made.

For more information visit Rik's website.

My Story. We're always interested in what you are working on. If you have a project that you're proud of, send it to us and we'll share it with the Jameco community. Send contributions to MyStory@Jameco.com.