|
What's the Missing Component? by Forrest M. Mims III |
Amateur electronic musician Joe Rhythm is planning a one-man video concert that he plans to post on YouTube. Controlling his array of instruments requires both hands and he wants to build a pressure-sensitive tone generator that he can control with a free finger or even an elbow or foot. Joe quickly whipped up a simple tone generator using parts from his bench stock. Since there wasn't enough time to order a pressure sensor, he improvised by making one from materials he had on hand. What did he use?

Figure 1. Simple pressure-controlled tone generator.
What is the pressure sensor concealed behind the puzzle piece? Before revealing the answer, here are some hints:
Figure 1 shows the the circuit. The 555 is connected as a pulse generator having a pulse repetition rate controlled by R1, C1 and the pressure sensor. This means the pressure sensor is a resistor whose resistance is controlled by pressure.
What is the pressure sensor behind the puzzle piece?
Click here to see the correct the answer.