Product Update: Solar Power Solutions
|
By: Robert Cong – Product Marketing Manager
As we approach spring, the sun should be shining down upon our heads on a more consistent basis. While most people may think it's time to pack away those winter clothes and start thinking about hitting the beaches, you may also want to start thinking about how to take advantage of the sunlight in a different way with the new line of solar products from Himin and Power Mate. Alternative energy is making big changes to the way we live our lives. It's affecting everything from the way our cars work to the way electricity is generated in our homes. Solar energy is one of the many technologies used to create electricity without releasing as many emissions as coal or oil. It is also one of the easiest methods that can be added to your own home to save you money on your electricity bill every month. |
|
![]() Part No. 2128569 25W Solar Panel with MC4 connections |
Part No. 2129191 MC4 Cable Adapters for Himin Solar Panels |
Solar charge controllers are used to regulate the amount of charge going into the battery from the solar panel. You never want to charge batteries without a charge controller because there is a high possibility of overcharging the battery, causing it to damage and possibly explode. The Power Mate charge controllers also come in 3 different ratings: 5A, 15A, and 20A maximum output current. They work in both 12V and 24V solar photovoltaic systems and even have the ability to be set in light-control mode so they automatically turn off when the sun goes down. Be sure to have a battery connected as well since the current from the solar panels goes straight into the battery. If an output load were connected at the same time, it would be powered directly from the battery.
![]() (5A version shown) Solar Charge Controller |
![]() |
If you're looking for a safe and easy way to recharge your batteries, you can start off by creating a small set-up with just a few parts as listed below:
Table 1: Parts List for Configuration
| Part Number | Description | Quantity |
| 2128569 | 25-Watt Solar Panel | |
| 2128593 | 5-Amp Solar Charge Controller | |
| 2129191 | Solar Panel Cable Adapter with MC4 connection | |
| 264049 | 12-Volt, 5 Amp-Hour Rechargeable Lead-Acid Battery | |
| 232602 | 14-AWG wiring | |
| 489694 | Quick-Connect Terminal Connector |
Using these parts, enough charge was delivered to an empty battery in approximately 4 hours of charging to brightly run a LED Christmas tree for 8 straight hours of standalone operation. If you would like to run an appliance that uses AC voltage, you will need an inverter. Just make sure the output of your panels is enough to power the inverter itself.
So as you're enjoying the sunlight this spring, think about helping out Mother Nature as well. Doing your part to reduce the amount of emissions released into the atmosphere is important for both the environment and your health. In the process, you will save some serious cash down the line and even learn a few things about solar power. It's a win-win-win situation.
Robert is a graduate from Cal Poly, San Luis Obispo in Electrical Engineering. He is originally from Lincoln Heights in Los Angeles, CA and currently resides in Belmont, CA where he works as a Technical Copywriter/ Product Manager for Jameco Electronics. His interests include sports, movies, music, and playing with cool, new gadgets.