Bluetooth Headset Hack

By Instructables contributor dex3844

Bletooth Hack
Instructable Logo

Do you want to play music from your computer on the stereo? We found this Bluetooth hack on Instructables and loved it. Here's what dex3844 wrote:

I came up with this Bluetooth hack to use with my computer and stereo, which doesn't have USB support but has stereo jack audio input - a DIY streaming audio project. I had a no longer functioning Bluetooth headset and hacked it to include a stereo jack. Now I just plug it in to the stereo and play the tunes (audio streaming)!!

Step 1 - Schematic

This is the circuit diagramThis is the circuit diagram


Step 2 - Parts and Tools Required

Required tools and parts Required tools and parts


You are going to need:

1. Bluetooth Headset
2. Stereo jack (3.5mm)
3. Soldering iron
4. Solder
5. Hot glue gun
6. Thin wire
7. Pliers/stripper/cutter
8. and of course a Bluetooth enabled computer.

Step 3 - Disassemble headset

Take the cover off Required tools and parts
Take the cover off and be careful with the small wires inside, it is easy to pull them out of their contacts. Strip off the casing of the stereo jack if needed.

what you should be leftThis is what you should be left with.


Step 4 - Wiring your hack

Wiring your hackWiring your hack


Solder two wires to the stereo jack by bridging the top two connections for left and right (black wire), then ground wire on third connection (white wire).

When you bridge the two top wires, solder that wire to one of the wires from the headset, then solder the other wire (ground) from your jack to the other wire from your Bluetooth headset.

Because this is a Bluetooth headset, there are only two wires (mono output instead off stereo left and right).

You might also want to snip off the microphone wires for privacy, but I didn't because I actually need that microphone for future hacks.

Make a small hole on the headset cover


Make a small hole on the headset cover.
Insert the stereo jack and secure it with hot glue.

Solder the wires


Solder the wires from the stereo jack to the headset wires.
Be very careful, it is easy to pull out the wires which I did.

Step 5 - Finishing touches

Put the cover back


Put the cover back and you have a finished product - Ta Da!

Your Bluetooth


Plug in your headset to the input (female stereo jack) of the stereo.
Turn it on and pair headset to your computer.
Play some music and enjoy!

Ideas for future improvements:

1. Write a computer program to include voice control so you can change music or switch off the computer from another room using a voice command.

2. Hack the stereo to charge the Bluetooth headset without unplugging it.

To view the entire story click here.


Jameco welcomes the contributions of its customers. Frankly, we think what you write is more interesting than anything we could write. Share your electronic component story, project, or challenge, and we'll share it with the world. Send your story to MyStory@Jameco.com