My Story: Build a Robot That Hides When He Gets Shy.

By: Ezra Velazquez

Rodney the Red Monster is a little shy of humans, the weirdest creatures in the known universe.


Red Monster
Background:

In the depths of Southern New Jersey there lives the mythical Jersey Devil, a monster so fierce and revered that no one dares travel to its swamps. I was ready to find the worst, and instead found Rodney.

How It Works:

A proximity sensor, built onto the base of the robot, checks for objects within a predetermined range every 1 second. If an object enters the sensor's range, the neck of the robot collapses into its body. This action is achieved by choreographing the movement of the base and middle servos, which act as the robot's neck joints. Once the object leaves the sensor's range, the robot "pops" its head back out by powering the two neck servos.

The top servo motor, which is the smallest of the three, moves the eyes of the robot back and forth when the neck is fully elongated. The servo motor moves the eyes back to their original position when an object enters the sensor's range.

The sound module plays audio clips while an object is outside the sensor's range. When an object gets within range, the audio track stops.

Testing the electronic components




Building The Robot

Construction:

The skeleton of Red is made of (3) three scrap pieces of wood found at the ITP shop. The neck is made of thin aluminum sheet strips. The body cavity is made of (2) two oatmeal barrels. The fur is made of "fancy" red yarn (that's what the store calls it, I like it because it feels, well, furry). The extremities are made of styrofoam and tube cleaners.

Notes:

The LEDs are used as status lights.
Green LED lights up when the audio-module is playing files.
Red LED gets brighter as an object gets closer to the proximity sensor.
The potentiometer is used to set the signal strength from the audio module to the LM386N chip.

Parts list:
(1) Arduino
(1) LM386
(1) Audio-Sound Moule - SOMO-14D
(1) Infrared Proximity Sensor Long Range - Sharp GP2Y0A02YK0F
(2) Servo - Large Full Roation
(1) Servo - Small
(3) TIP120
(1) LD33CV
(1) Speaker - 0.5W 8Ω
(2) 220 µF capacitor
(1) 100 µF capacitor
(1) 10 µF capacitor
(1) 1K resistor
(2) 470Ω resistor
(2) 10Ω resistor
(1) 10K potentiometer
(1) Red LED
(1) Green LED

Resources:

ITP Physical Computing Tutorials
Audio-Sound Module Datasheet
LM386 Audio Amplifier


Solutions:

Arduino Code

Breadboard Diagram
Schematic Diagram





Project created by: Ezra Velazquez.
Ezra is currently a Master's candidate (2012) for Interactive Telecommunications at New York University.
He obtained his Bachelor's (2010) on Computer Science and Cinema & Media Studies at Carleton College.

http://ezraezraezra.com