Flicker-Free LED Lighting Power Applications
What is Lighting Flicker?
Flicker is a noticeable variation in luminance between cycles. The fluctuating light causes luminaries to flicker. Human eyes can typically detect flickering at frequencies lower than 100 Hz. A frequency exceeding 100Hz is difficult for human eyes to perceive.

Since traditional lamps use AC mains as their input source, 50Hz is the frequency at which the current is conveyed. Peak and trough voltage fluctuations are observed at the output. As a result of the absence of a control loop in electronic ballasts and the periodic variations of AC power, the luminance of the lamp varies with the frequency of the AC main, which is about two times the frequency of the electronic ballast.
Modern farm lighting has reached the stage of intelligent control as a result of its constant growth. LED lighting for poultry is distinct from conventional commercial lighting. It is essential to take into account the physiological properties of chickens. Light intensity, duration, and spectrum have a significant impact on the development of poultry. Under optimal conditions, led lighting can stimulate the appetite of chickens, increasing their intake and promoting their growth. Thus, the production of "meat and eggs" is increased. However, as poultry is extremely sensitive to light, LED drivers with PWM dimming are unsuitable for dimming applications involving poultry.



Contact us today to discuss how we can help with your business requirements. For more information or to request product samples and quote request please send an email to [email protected] or call 1-800-794-9100.
After 40 years in business, MEAN WELL has been designing power solutions to some of the world's most recognizable enterprises. Jameco Electronics carries the majority of MEAN WELL's products and has access to all power supply models currently in production.