How to Build Your Own Non-contact Voltage Detector
By Kiran DawareDescription: Non-contact Voltage Detector
Skill Level: Beginner
Assembly Time: 1 hour or less
Electricity can cause serious injury or even death which is why safety must come first when working with electricity or electrical devices. In order to avoid injury, prior to starting work on an electrical box such as an AC mains switch-board or a power supply, for example, you must first verify there is no AC voltage. If you can't completely isolate your device from the supply wires, how can you be sure that there's no voltage remaining? Enter a non-contact AC voltage detector.
There are several options available on the market and they range in price, but in true DIY fashion, with this kit you are able to quickly and easily create your own non-contact AC voltage detector in less than an hour.
Required Tools:
Soldering Iron
Solder
Drill and drill bits (for making holes in the box)
Copper Wire
Cutters (for copper wire)
Adhesive Tape
Circuit Diagram
Purchase the Non-Contact Voltage Detector Kit.
The kit includes:
Qty. | Part Description | Mfr. Part No. |
3 | Transistors | 2N3904 (FSC) |
1 | Resistor 1.0 MΩ | CF1/4W105JRC |
1 | Resistor 100KΩ | CF1/4W104JRC |
1 | Resistor 200Ω | CF1/4201JRC |
1 | LED, Red | UT1871-81-M1-R |
1 | Buzzer | TDB05LFPN |
1 | Switch | T100T1B1A1QN |
1 | Prototype Builder | G/S(PCB228)-R |
1 | 9V Battery | ALK 9V 522 |
1 | Battery Snap | BC6-R |
1 | Case | H2853-R |
How Does a Non-contact AC Voltage Detector Work?

This non-contact AC voltage detector uses NPN type transistors in order to detect voltage. A transistor has three terminals - collector, emitter and base. Collector to emitter current is controlled by the base current. When there is no base current, no collector to emitter current flows. Thus, a transistor acts as a switch. It can be 'ON', it can be OFF or in-between.
The ratio of collector current to base current is known as the gain of a transistor. Normally, gain of 2N3904 is about 200, i.e. collector to emitter current can be as high as 200 times the base current. If we connect the output of one transistor to the base of another transistor, the total gain would be multiplication of the two i.e. 200x200 = 40000. Thus, if we connect three transistors in such configuration, the total gain would be 200x200x200 = 8,000,000. Therefore, an extremely small signal can be used to switch ON a normal circuit by using such configuration of transistors.
In our circuit, an antenna (copper wire) is connected to the base of first transistor. When we place this antenna near an object that is AC energized, a small current gets induced into the antenna due to electromagnetic induction. This current triggers the first transistor and output of the first transistor triggers the second and third. The third transistor switches ON the LED and buzzer circuit, indicating that AC voltage is present.
Building Your Own Non-contact AC Voltage Detector
Use the following circuit diagram as a reference to place the components on the Printed Circuit Board (PCB).

Mount the components on the PCB and solder them one by one in the appropriate places as per the circuit diagram.
Connect one terminal of the copper wire and to the base of the first transistor. The copper wire will act as an antenna. Tip: For improved sensitivity use about 10 to 12 cm of wire.
Make two holes in the case - one for the switch and another for removing the copper wire. Attach the switch to the box.
Put the circuit inside of the box. Take the antenna wire outside, twisting it into a spiral shape. Attach it to the box using adhesive tape.
Connect the wires to the switch as per the circuit diagram.
Attach the wires of the 9V battery holder to the circuit according to the schematic. The battery symbol should have a plus on one side for polarity.

Once complete, you are ready to detect whether or not AC voltage is present. Switch on your non-contact AC Voltage Detector and take it near the object you would like to know whether voltage is present or not. If you hear the buzzer, there is AC voltage present, if not, no AC voltage remains.
Watch the video:
Keep yourself safe so you can keep on building! This kit is compact and portable so there's no need to worry about AC voltage. You can gain a little extra electronics experience and focus on your projects knowing you don't need to worry about remaining voltage.

If you have an electronics project you would like to share, please email us at [email protected].
Kiran Daware is an electrical engineering student as well as an enthusiast blogger. He likes everything electrical and writes about electrical engineering basics at www.electricaleasy.com