Arduino Portenta Breakout Board

Maximize the power of the Portenta


Arduino Portenta Breakout Board


Makers and engineers who work with hardware can use the Arduino Portenta Breakout Board to make prototypes of devices and test their connections and capacity in the Portenta family of boards. It lets you connect and test external hardware components and devices quickly and easily in the lab by making all high-density connectors' signals available one by one. This makes it easier to connect and test hardware components and devices. It cuts down on the time it takes to make an industrial-grade automation solution. The Portenta Breakout board can be used to teach technicians how to work with industrial-grade control and embedded systems at the start.

Portenta Breakout Application Examples

Product Development

The Portenta Breakout board cuts down on the time it takes to make industrial-grade automation solutions that use the Portenta line.

OpenMV

Connectivity to the OpenMV Global Shutter Camera Module is available on the Portenta Breakout board, making it easy to build machine vision applications with the Portenta family of boards.

Technical Education

The Portenta Breakout board can be used to teach technicians how to work with industrial-grade control and embedded systems at the start.

Arduino Portenta Breakout Board Pinout


The Portenta Breakout shortens the time it takes to make industrial-grade automation solutions based on the Portenta line. Designed to help hardware engineers and makers who want to make their own device for the Portenta family boards or connect other devices to the Portenta family boards (e.g. the Portenta H7). Use all the high density connector signals of the Portenta one at a time to connect external hardware parts and devices in the lab.

Rapid Development for machine Vision

Connectivity to the OpenMV Global Shutter Camera Module is provided on the Portenta Breakout, allowing for rapid development of machine vision applications alongside the Portenta family.

Portenta H7 and Global Shutter Camera Module
Example of a Portenta H7 and Global Shutter Camera Module installation.


Test External Hardware and Devices

The Portenta Breakout makes it easy to debug your computer by connecting to the JTAG port. It also lets you look at the bus lines through the breakout pins. In addition to the breakout pins, the Portenta Breakout has Ethernet, USB, SD, a coin cell, a power button, an external power supply, an OpenMV camera socket, and configurable boot modes. It also has a coin cell, a power button, and an OpenMV camera socket.

Portenta Breakout Features

  • Power ON Button
  • Boot mode DIP switch
  • Connectors
    • USBA
    • RJ45 up to 1Gb/s
    • Micro SD card
    • OpenMV shutter module
    • MIPI 20T JTAG with trace capability
  • Power
    • CR2032 RTC Lithium Battery backup
    • External power terminal block
  • I/O
    • Break out all Portenta High Density connector signals
    • Male/female HD connectors allow interposing breakout between Portenta and shield to debug signals
  • Compatibility
    • Standard Portenta High Density connector pinout
  • Safety information
    • Class A


Click here to learn more about the Portenta H7 Microcontroller

Click Here to Review all Arduino Products