Electronics Puzzler: Wireless Chime
By Forrest M. Mims III
What's the Power Supply?
Big Bucks Bank needs a totally wireless, stand-alone means to sound a chime when a visitor enters the lobby of its bank during business hours. No wires can be connected between the foyer and the inside of the bank. The system and its 6-volt power supply must be installed in the foyer and should have a working life of at least 15 years. The solution is shown inThe circuit sends a pulsed IR signal from the foyer of the bank, through the glass door and to a receiver inside the bank that activates a chime when a visitor steps on a floor switch (S1) in the foyer. The circuit draws current only when S1 is closed, and its power supply has a life of at least 15 years.
What is the 6-volt power supply concealed behind the puzzle piece?
Puzzler Hints:
The circuit draws current only when a customer enters the bank foyer and steps on a switch mat, usually for a fraction of a second.Lithium batteries might work, but maybe not for a full 15 years.
Power is dissipated in the floor switch when a visitor steps on it, but this power is not used to power the circuit above.
The system needs to work only during banking hours (9:00 AM to 3:00 PM).