Build A Thermometer Kit
Assembly Time: 1 to 2 hoursDifficulty: Beginner
Designer: Austin Mier
Build a modern thermometer that measures a change in resistance within a circuit.
Required Tools and Components:
soldering iron
soldering iron stand
solder
wire cutters
Part Description | Part Number | |
10KΩ Potentiometer | 3386P-1-103/63P103 | |
100KΩ Potentiometer | 3362P-1-104LF-VP | |
1KΩ Resistor | CF1/4W102JRC | |
330Ω Resistor | CF1/4W331JRC | |
220Ω Resistor | CF1/4W221JRC | |
LED array | LTA-1000HR | |
LM3914 driver | LM3914N-1 | |
Green LED (10 pack) | LG3330 | |
Thermistor | NTC-502-R | |
9V battery | ALK 9V 522 | |
9V battery plug | BC6-R | |
PCB | — | |
DIP Switch | 206-2-VP-R |
How does this circuit work?
This circuit works off of a variable resistor called a thermistor. As temperature increases or decreases, the resistance of the thermistor changes. In this circuit, the thermistor has a negative temperature coefficient (NTC); as the temperature rises, the resistance of the thermistor decreases by a certain percentage for every unit of temperature. This is useful because in our circuit, we have a potentiometer in series with the thermistor and as the resistance of the thermistor drops, the voltage drop of the potentiometer rises in relation to the voltage drop of the thermistor. This is because of a certain give and take between components in a series configuration.In series, the components together have a voltage drop equal to the power source voltage. However, each component drops only its share based off of resistance of the voltage. For example, our potentiometer and thermistor have a combined voltage drop of 9v from the battery. When the potentiometer is at 5,000 Ohms and the thermistor is at 5,000 Ohms, each component drops 4.5v. Now if the temperature increases, the thermistor resistance may drop to 2,500 Ohms while the potentiometer is still 5,000 Ohms. This means the potentiometer will now drop 6V, a 1.5V increase. We can then measure the voltage drop across the potentiometer to see changes in temperature.
The LED array is built into a voltmeter circuit using the LM3914. The two potentiometers can be used to calibrate the readout and sensitivity of the LED array The green LED is simply used to state if the circuit is on or off.
The schematic for our thermometer circuit is below:

Electronics Projects Recommendations
If you decide to use a rubber band to hold the battery, add a small notch in the PCB directly above the two potentiometers to keep it from slipping.We also recommend having a multimeter on hand because it is handy if troubleshooting is necessary. One multimeter we recommend is Jameco digital multimeter with LCD display.
Helpful Tips
1. LEDs have a specific direction - long side to positive. If the components are installed backwards, the circuit will not work and pieces may fail.
2. Do not trim leads before board is soldered and tested.
3. Keep the soldering neat, but don't get frustrated with this project if your soldering is not perfect.
4. Solder the smallest components first. This is much easier than soldering larger components in first and then squeezing in the small pieces.
5. Don't solder things outside of the PCB first. I know this is obvious, but if you accidentally damage a component, the whole circuit will not work as designed and the component may not fit into the PCB.
What can you measure?
This thermometer works best when measuring mild temperatures, from 0-50 degrees Celsius. The thermistor takes a few seconds to reset and will display change gradually.Directions
Refer to the PCB pattern below*.
Click for large image
Insert the components on the top of the PCB and solder on the bottom. The placement for the components on the PCB is as follows:
BAT1 D1 R1 R2 R3 R4 R5 R6 R7 R8 R9 R10 R11 R12 R13 R14 R15 U1 U2* U3 |
9v Clip Leads Green LED 100kΩ Potentiometer 10kΩ Potentiometer 220Ω Resistor 220Ω Resistor 220Ω Resistor 220Ω Resistor 220Ω Resistor 220Ω Resistor 220Ω Resistor 220Ω Resistor 220Ω Resistor 220Ω Resistor 1kΩ Resistor 330Ω Resistor 5kΩ Thermistor LM3914 LED Array DIP Switch |
*Note: The first revision of the PCB Silkscreen shows U2 (LED array) incorrectly. The notch should be at the opposite side. When installed, the notch on the LED array should be near the outside edge of the PCB.

Identify the different values of the resistors by the colored bands.
• 330Ω resistor has bands: ORANGE, ORANGE, BROWN, GOLD
• 220Ω resistors have bands: RED, RED, BROWN, SILVER
• 1000Ω resistor has bands: BROWN, BLACK, RED, GOLD
Clip excess length, from the leads of the components on the back of the PCB. Only do this after the pieces are soldered in securely.
Connect the 9V battery once everything is soldered to the PCB. Using the DIP switch on the PCB, turn on the thermometer. The green LED should light. By adjusting the potentiometers, you can calibrate the thermometer.
Austin Mier, an engineering student at University of New Mexico, recently worked at Jameco Electronics as an intern.
READER COMMENTS:
The description should have mentioned how to calibrate. An easy, and pretty good, way is: Ice and water slush to set 0°C and boiling water (if the thermistor will stand it) for 100°C. If there was interest I could even give a formula that would minimize the back and forth. There are also much higher grade thermistors accurate to .1°C that are used in the medical thermometers.
Respectfully, using a thermistor for a temperature sensor is not terribly accurate or stable. Perhaps you would consider using the LM24 for this purpose. The OPA342 is actually optional, but adding a little gain to the LM34 will make the entire system less sensitive to noise, and to thermal effects on the potentiometers. With these settings, the output of the OPA342 will be 200mV/°F. While the LM34 can go to negative temperatures, doing so will require a dual supply.
The fundamental theory behind the design is flawed. The accuracy of the measurement is wildly dependent on the supply battery voltage, the device itself used to measure temperature is so non-linear with temperature as to be absolutely worthless as a thermometer. Not intended to replace your thermometer.