History of the Power Cord
Powering your devices is as simple as plugging something into a wall outlet. The power cables that power your everyday devices are undeniably vital. There are different power cord types, including AC power cords, USB cables, and high-voltage cables, each designed for specific applications and environments. These power cables can be found everywhere, from portable devices like smartphones, power banks, and tech devices to heavy-duty machinery such as industrial equipment and large appliances.
These power cords are vital in transmitting electricity for charging, running, or controlling devices. However, creating such an invention took some time and lots of effort. So, what is a power cord and who invented the power cord? Here are some insights about the history of the different types of power cords, from the invention of vulcanized rubber to more modern means of insulation and conduction.
Thomas Edison’s First Power Distribution System
In 1882, Thomas Edison pioneered the first power distribution system in New York City. His innovative system utilized copper rods wrapped in jute and placed in rigid pipes filled with a bituminous compound. Copper, which continues to be the preferred electricity conductor today, offered an impressive 100% conductivity – a close second to silver’s remarkable 105%.This high conductivity, combined with copper’s relative affordability and malleability, solidified its vital role in the rapidly developing world of electricity at the time. As the demand for electricity surged, so did the necessity for efficient and reliable power distribution methods, including power cord types. Edison’s groundbreaking system laid the foundation for future advancements in power cable technology.
Vulcanized Rubber and Cable Insulation
While Charles Goodyear patented vulcanized rubber in 1844, this versatile material wasn’t applied to cable insulation until 1880. The process of vulcanization, which involves treating natural rubber with heat and sulfur, significantly enhanced the rubber’s durability, strength, and resistance to temperature changes—properties that proved invaluable for cable insulation.Vulcanized rubber quickly gained popularity due to its insulating benefits, effectively protecting electrical conductors from environmental hazards. Its widespread use continued until the 1930s, when technological advancements in power cord types and evolving industry demands began to reshape the landscape of cable insulation materials.
Armored Cables and the Shift to Aluminum
In 1906, armored cable was introduced, although its high cost was initially prohibitive. By the 1960s and 70s, aluminum wire became a more affordable alternative to copper. However, aluminum was later deemed unsafe due to corrosion issues, casting a shadow on its viability as a safe and dependable conductor.The rise and fall of aluminum as a preferred conductor material underscored the ongoing quest to balance cost-efficiency and performance in power cable technology. This delicate balance continued to shape research and innovation, paving the way for the advanced solutions we see today in different types of power cords.