Get 6 times the processing capacity of previous models with Jameco's selection of Raspberry Pi Boards. Choose from the raspberry Pi 2 or Pi 3 models. The third generation Raspberry Pi has an upgraded Broadcom BCM2837 processor, a powerful 64-bit ARM Cortex-A53 based quad-core processor that runs at 1.2 GHz. All of these improvements lead to a 50-60% increase in performance in 32-bit mode when compared to the Pi 2 and nearly a 10-fold increase over the original Raspberry Pi.