Assembled Pi T-Cobbler Plus - GPIO Breakout for Raspberry Pi
This is the assembled version of the Pi T-Cobbler Plus. It only works with the Raspberry Pi Model Zero, A+, B+, Pi 2,Pi 3! (Any Pi with 2x20 connector)
The Raspberry Pi has landed on the Maker World like a 40-GPIO pinned, quad-USB ported, credit card sized bomb of DIY joy. Now is a good time to upgrade your set up and accessorize using all of the 40 pins.
That's why we now carry the Adafruit's Assembled Pi T-Cobbler Plus (Breakout + Cable) for Raspberry Pi. This Cobbler is in a fancy T-shape, which is not as compact, but is a little easier to read the labels.
The T-Cobbler Plus is an add on prototyping board specifically designed for the 2x20 connector-type Raspberry Pi and can break out all the power, GPIO, I2C and SPI pins from the 40-pin header onto a solderless breadboard. This set will make "cobbling together" prototypes with the Pi that much easier.
Each order comes with a 40 pin ribbon cable and assembled T-Cobbler Plus. You can plug the 40-pin GPIO cable between the Pi computer and the T-Cobbler breakout. The T-Cobbler can plug into any solderless breadboard. The T-Cobbler PCB has all the pins labeled nicely so you can go forth and build circuits without keeping a pin-out printout at your desk. We think this will make it more fun to expand the Pi and build custom circuitry with it.
Designed for use with any 2x20 connector Raspberry Pi. No soldering required!
The Raspberry Pi, solderless breadboard, breadboarding wires, cables, components, power supply, etc are not included! We stock many of those items, so check those out as well!