The Official Arduino Starter Kit - Uno R3 Included

You may also like:
DFR0100 DFR0100
DFRobot
DFR0107 DFR0107
DFRobot
KK6 KK6
Jameco Valuepro

$110.30 ea

182 In Stock
More Available – 7 weeks


  • Jameco Part no.: 2171188
  • Manufacturer: Arduino
  • Manufacturer no.: K000007
  • HTS code: 8542310000
  • No datasheet available. Please review the tabs below for product specifications.
  • Web Exclusive

The Arduino Starter Kit

This kit walks you through the basics of using the Arduino in a hands-on way. You'll learn through building several creative projects. The kit includes a selection of the most common and useful electronic components with a book of 15 projects. Starting the basics of electronics, to more complex projects, the Arduino Uno starter kit will help you control the physical world with sensor and actuators. The Arduino Software is downloadable and supports Windows, Mac OS X and Linux (32-bit/64-bit).

Product Note: The USB cable assembly in the Uno R3 starter kit mates easily but does not UN mate easily. Arduino is aware of the issue and suggest the cable be removed by holding the USB connector on the Arduino board and while pulling shifting the plug side to side until removed.

The projects in the Arduino starter kit are:
  • 01 GET TO KNOW YOUR TOOLS - An introduction to the concepts you'll need to use this kit
  • 02 SPACESHIP INTERFACE design to control panel for your starship
  • 03 LOVE-O-METER - Measure how hot-blooded you are
  • 04 COLOR MIXING LAMP - Produce any color with a lamp that uses light as an input
  • 05 MOOD CUE - Clue people in to how you're doing
  • 06 LIGHT THEREMIN - Create a musical instrument you play by waving your hands
  • 07 KEYBOARD INSTRUMENT - Play music and make some noise with this keyboard
  • 08 DIGITAL HOURGLASS - A light-up hourglass that can stop you from working too much
  • 09 MOTORIZED PINWHEEL - A color wheel that will have your head spinning
  • 10 ZOETROPE - Create a mechanical animation you can play forward or reverse
  • 11 CRYSTAL BALL - A mystical tour to answer all your tough question
  • 12 KNOCK LOCK - Tap out the secret code to open the door
  • 13 TOUCHY-FEEL LAMP - A lamp that responds to your touch
  • 14 TWEAK THE ARDUINO LOGO - Control your personal computer from your Arduino starter kit
  • 15 HACKING BUTTONS - Create a master control for all your devices!
Once you've mastered this knowledge, you'll have a palette of software and circuits that you can use to create something beautiful, and make someone smile with what you invent using the Uno R3 starter kit. Then build it, hack it and share it. Because Arduino is you!

What's in the Arduino starter kit is listed below. Click on the name of the component to download the datasheet of the part. This document will describe the design and functionality of the component. Look at the Arduino Starter Kit gallery.

If you need support when working with the Arduino Uno starter kit, please visit the dedicated area in the Arduino forum section.

Report a problem
Suggest a product
Specification Value
Design LevelBeginner Kit
Piece Count217


Report a problem
Suggest a product