DIY Arduino Uno Mini LE Weather Station
By: Pranav PuttaWith this project, you'll find the fundamental instructions for building a circuit board that will eventually show the ambient humidity and temperature on an LCD screen. For those who have worked with Arduino before, this is a great project using the Arduino Mini LE microcontroller board. It is encouraged that you make this kit your own by modifying the project to your liking and expanding upon the instructions.
To get started, it helps to have a fundamental understanding of the components that make up a breadboard and an Arduino Uno Mini. Take a look at the following diagrams:
Arduino Uno Mini Limited-Edition Layout
Breadboard Layout
Digital Temperature Humidity Sensor Module Layout (DHT 11)
Note: Double check the pins on your DHT 11 sensor, as some have different layouts than the image below.
Serial I2C TWI Module
16x2 LCD Display
The parts you need to get started:
- Solderless Breadboard (6.5'' x 2.5'')
- Digital Temperature Humidity Sensor Module
- 16 x 2 LCD
- Serial I2C TWI Module
- 40 x 20 cm Male to Female Jumper Wires
- 65 x Male to Male Jumper Wires
- Arduino Uno Mini LE
- Screwdriver
STEP 1 Attach the 16 x 2 LCD to the breadboard using the pins on the backside as shown below.
Step 2: Attach the Digital Temperature Humidity Sensor Module as shown below. Refer to the DHT 11 layout above for what each pin is labeled as (Double check online as some DHT 11 sensors have different pin layouts). Attach a male-to-male jumper wire from the VCC node to the negative (-) rail of the breadboard. Attach a male-to-male jumper wire from the Data node to the A0 port on the Arduino Uno Mini Limited Edition. Attach a male-to-male jumper write from the GND node to the positive (+) rail of the breadboard. Refer to the images below for clarity:
Note: You can find the ports on the Arduino Mini Limited Edition labeled underneath it.
Step 3: Attach the I2C TWI Module above the pre-soldered pins of the LCD. Attach 4 male to female jumper wires to the I2C TWI Module. Refer to the images below.
Step 4: Wire the GND port on the I2C TWI Module to the negative (-) rail on the breadboard, the VCC port to the positive (+) rail, the SDA port to the SDA port on the Arduino Uno Mini Limited Edition, and the SCL port to the SCL port on the Arduino Uno Mini Limited Edition. Refer to the images below:
Step 5: Connect the 5V port on the Arduino Uno Mini Limited Edition to the positive (+) rail on the breadboard. Connect the GND port on the Arduino Uno Mini Limited Edition to the negative (-) rail on the breadboard. Refer to the images below:
Step 6: Connect the Arduino Uno Mini to your laptop/computer. Open the Arduino IDE and use the code which is linked in the article below (Use the article as a guide to this project as well). You will need to download the libraries linked below as well. After you’ve completed these steps, you may upload the code to your Arduino.
Libraries Link
Code Link
Weather Station Demonstration Photo
Note: You may need to use a screwdriver to twist the blue square on the I2C module to change the contrast of the LCD if it displays a blank screen.
About the Author
Ryan Winters serves as Product Manager at Jameco Electronics, an organization based in the San Francisco Bay Area of California, where he was born and raised. A self-directed learner, Mr. Winters dedicates his personal time to refining practical skills through hands-on work with automobiles, computers, and electronic devices, as well as experimental robotics projects. Through these diverse areas of technical exploration and problem-solving, he further develops the analytical and creative abilities that serve him well in his professional role, where he applies expertise gained from years of independent study and tinkering to benefit Jameco Electronics and their customers.